I have built a connection between simpleBLEcentral and simplebleperipheral. The simplebleperipheral will delay 20 seconds to enter GAP_LINK_TERMINATED_EVENT When I power down the simpleplecentral. I modify the value DEFAULT_DESIRED_CONN_TIMEOUT from 1000 t0 100. It also need to wait 20s to enter GAP_LINK_TERMINATED_EVENT.How can I enter GAP_LINK_TERMINATED_EVENT immediately after the link loss. Thanks.