Hi,
I want to achieve OOB pairing between two CC2541 devices (One acting as central and the other acting as peripheral) using NFC. My use case is as follows:
- I have two boards based on CC2540 DK. Each board has CC254x, NFC chip, battery, etc
- Initialize the two boards (CC254x, BT Stack, NFC, etc).
- Tap the two devices.
- The central should get information about the address of the peripheral and we should be able to do OOB pairing. (There should be no need of Bluetooth discovery or entering PIN code)
- Switch off NFC so that remaining communication can happen on BLE link.
I would like to know which NFC chip would be appropriate for this considering that the boards are battery powered and we don't want a big impact on the battery life.
I already looked up RF430CL330H, but it seems that this chip can support only pairing with a mobile phone.
Could you help me with the part number of the chip that I can use for my use case and if any sample software is available for CC254x.
Thank You,
Naresh