There is a documentation bug in TI BLE Vendor Specific HCI Guide version 1.4 on page 76, section 12.9. The description of the GAP Terminate Link Request command packet is wrong. In the Command Parameters section, there shouldn't any reason parameter. This is a mix between the command and the event. The GAP link termination event contains a reason parameter as far as I know.
If I am wrong, then the first table is then wrong, as there is no reason parameter described.
Can someone give me more details on the correct command packet format? I am struggling to have the link terminated properly here and something seems to not working.