Hi Sir,
I am developping a project based on hostTestApp with CC2540. An external MCU is used to control the BLE SOC over HCI interface(UART). There are two LEDs used to indicate the system state. However, becasue of the limit number GPIOs on MCU side, we want to put the LEDs on BLE SOC side. Then according to the "TI_BLE_Vendor_Specific_HCI_Guide",we do not find the command to do this(control a GPIO). Although there are some other command like "HCI_EXT_AdvEventNoticeCmd " and "HCI_EXT_ConnEventNoticeCmd" which can be used to trigger a task with such event,we need to more states on LEDs.
Then what should we do for this?
Another question, for HCI over UART, is it more stable for UART with CTS/RTS compared to the 3-wire connections(UART_TX/RX/GND)?