Hi,
When I tried different sets of connection parameters then I observed that it also changes connection period (3.68ms as in below snapshot) based on the connection interval that we set. If the connection interval is short then connection period is also short and similarly it shows the behavior for longer connection interval. Is it possible to keep the connection period shorter even after we configure longer connection interval ? Is there any link layer settings available in BLE stack.