Hi,
I am trying to put the CC2541 into the lowest power mode, but I am still getting much higher current consumption and the device keeps waking up very frequently.
1. Here's the measurement with the CCDebugger attached. I am expecting the device to go in the P3 state and should consume 0.5uA, but instead the lowest I see is 22uA. So it's not even P2 and it can't be in P1. But then every ~89.2us it goes up to P1 and draws 270uA.
2. With the CCDebugger attached, I am getting better current, but still nowhere close to P3/P2.
Now the low is ~18uA (still very similar to the 22uA that I was getting earlier). It doesn't wake up and go to P1 as often, but still does it every 1.24msec (vs 8.9usec).
So the questions
Q1: What could cause the SOC to consume 17 or 22uA instead of 1uA (in P2) and 0.5uA (in P3)? What could I do to reduce it down to 0.5-1uA?
Q2: What could cause the SOC to keep waking up ever 1.24msec? How do I prevent it from doing this?
Thanks in advance,
Chintan