We developed a test application using the SmartRF06 and the CC2650EM_5X5 for BLE based on the SimpleBLEPeripheral The project runs and can be debugged and stepped through. Our target PCB uses a CC2640 5x5, so I did not change any project settings.
Problem:
1) Our new CC2640 PCB loads, and the XDS100v3 debugger is stepping through the program but we are not seeing any advertising packets.
2) The current draw is 2mAmps.
3) I also loaded the SimpleBLEPeripheral app, and that appears to be running on the new PCB.
Question: How can I verify that the CC2640 system is actually running the BLE tx-rx portion?
Thanks,
Dan