Hi,
I have designed a custom board around CC2564 with TAS2505 amplifier for one of my BT application to be controlled by Mobile app which is functional. As i can't reveal lot of details about the design, i will try to explain the problem by taking a analogy.
Along with BT stack, i have my own application running on CC2564 which can toggle few GPIO's. As of now i can toggle GPIOs but i need to add conventionality to enable I2C on the stack. As a developer i can always flash the firmware using TI tools but at end user premises i am plan to do OTA (over the air update) using my mobile app.
1.Firstly is my thinking possible?
2. If so, how do i go about? Any documents from TI?
3. Do i require additional HW support on m y board to do the same?
4. When the firmware upgrade is in progress, does BT stack still stay alive to receive data from my App (basically new firmware)?
I know these might be very high level questions but i am not sure where to start from, hence asked it vaguely.
-Prashanth