I was able to configure an RF430CL330 IC per the instruction in the data sheet (table 30) for setting the data rate to something other than the default data rate of 106kpbs. Is there a way to confirm the NFC data rate that is being used in the communication? I try to read back register 0x2A78, but I'm not sure it is a readable location. If it is, it is always coming back 0x00 which is the default low rate of 106kpbs. I've attached a couple of log files from my attempt to set the IC to read/write at the high rate (847kpbs) only. Is there a way to confirm the mode I'm in by reading a certain register? Or is there an Android app that will report what rate a data transfer occurred at?