Hello,
I’m using the TI NFC sample project to develop my own adc measurement code. So my problem starts really in the beginning. If I just import the project and want to see how the sample code works for later debugging at the main function (where I want to put my code later) the debugger already failed with the error “MSP430: Can't Single Step Target Program: Could not single step device” This happens exactly when the sample project jumps into DeviceInit() function. So I’m not able to debug my code later at the main function if the sample code is already buggy. What I’m doing wrong?