Hi,
I am using the CC3000 with a STM32f372 microcontroller. My problem is that the interrupt is not happening after the First packet write to CC3000 device.
Here I am able to the get the response to the simple link start command.
I am requesting 0x01, 0x00, 0x05, 0x00, 0x00, 0x01, 0x00, 0x40, 0x01, 0x00, and I am receiving the response 0x02, 0x00, 0xFF, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00.
Which same response is given in ti CC3000 document, so I am suspecting my SPI transmit and receive both are working fine.
After receiving the first response from the CC3000 module I am not receiving the interrupt, so that tSLInformation.usEventOrDataReceived(which is set in the SpiReceiveHandler) is always low. Please anyone help me to solve the problem.
Regards,
KC.