Hi
i have a question about the connection between cc3000 and the router.
Based on the Basic_Application code i used Hyperterminal to send the commando : 01 is Smartconfig and it is ok.
03 menas Socket open, and i dont know if it is ok. When i tried sending a self-defined data (UDP) to the PC, i find that there is no Ip-address. and shortly after i type 04 sendingcommand it is showd "Done". But after 04 i still need to type my data informations, Ip Address and so on. I dont know if CC3000 already connected with my Router or not yet ? I have checked the code and i think the ucRxBuffer dosent recieve the data from Hyperterminal rightly. Downside i show a cutshot for Hyperterminal. Thanks for your answer.
Best regards,
Shagar