Hello all,
I have 2 questions:
1. I would like to know if there is a Simple Link WLAN event (similar to connected or disconnected events) that can signal that scanning process is done?
I do not want to wait the 900ms delay, but I would like to have a callback saying that scan has finished.
sl_WlanPolicySet(SL_POLICY_SCAN , ucpolicyOpt, (UINT8*)(policyVal.ucPolicy), sizeof(policyVal)); Delay(900);
2. I am having some issues with
#define SCAN_TABLE_SIZE 20 retval = sl_WlanGetNetworkList(0, SCAN_TABLE_SIZE, &netEntries[0]);
When the size is greater than 2, the function gets stuck. (waited more than 10 minutes each time).
When size is 1 or 2 I can increase index of net entries and I am able to get the list of the networks.
Do you know what could be the problem?
Thank you in advance,
Dobrin