I have the cc3200 and I'm trying to figure out a way to change parameters on the cc3200, like turn on an LED or change the SSID from a mobile device.
I've read the documents on HTTP server and the GET and POST, but this seems to relies on having an embedded wed page that has tokens. I would like to send an HTTP POST command and in the body of the request have a command that the cc3200 interprets as a command. The flow would be like this:
1) cc3200 goes into AP mode
2) Mobile device connects to cc3200
3)Mobile device send HTTP POST request and in the body has a string that says "Turn ON LED"
4)cc3200 receives this string and turns on the LED.
No embedded web pages involved. Can this be done? if not by HTTP, can using the UDP or TCP be used.
I would also use this to GET data from the cc3200 upon request.