Other Parts Discussed in Thread: CC2530, Z-STACK, SIMPLICITI
Hi
I have problem with my cc2530-cc2591 module ,my module designed respectively to TI design reference so as the BOM is respectively to TI BOM
I mad one change in my design as follow:
P1.1 change to P1.0 and change the registers as was recommended int TI AN078
and P0.7 to P0.5
"
1) P0_7 can be moved to any GPIO pin, and the macros below HAL_PA_LNA_RX_LGM() and
HAL_PA_LNA_RX_HGM() must be modified accordingly.
2) P1_1 and P1_4 are a subset of GPIO pins (only P1.0-P1.5) that can be configured to
support special RF observation output control signals. PAEN and EN of the CC2591 are
directly controlled by these signals via the radio core logic of the CC2530. See the CC253x
User’s Guide for more details. The user only needs to adjust the OBSSELx registers to
change the pin assignment "
the changes made according to TI
when I tried my Hardware it seems that the cc2591 doesn't do his job at all i got low power in the output
any advices pls ??