Part Number: CC2650DK
Hi,
I am using the document (swra446.pdf) that explains setting up environment to flash and debug apps on cc2650DK using Eclipse+GDB. Application is the simplest blink example.
Now, I've managed to build .bin file, but when I try to flash with SmartRF Flash Programmer, I get the following:
------------------------------------------------------------------------------------------------------
Texas Instruments SmartRF Flash Programmer 2 v1.7.5-windows
-------------------------------------------------------------------------------
Reading file: C:\EclipseEABI_Workspace\cc26xxTest\bin\cc26xxTest.bin.
File size: 131068 bytes.
1%
2%
Number of assigned pages: 8.
About 20 percent of the file contain assigned code.
Start flash erase ...
OK
Start flash programming ...
0%
0%
12%
99%
Reset target ...
Flash loader reported an error (4)
Error occured at addr: 0x0001FFA8, writing 68 bytes.
Failed to write 68 bytes to address 0x0001FFA8.
OK
---------------------------------------------------------------------------
The same happens when I try to flash directly from SmartRF Flash Programmer, i.e. not using Eclipse.
Linker allocates 88 bytes of Flash starting at 0x1FFA8 - for CCFG, so I guess there is some problem with this area, but I do not understand why it fails.
If someone has experience something similar, I'd be gratefull for inputs.
Thanks,
Goran