Hi all
I am fairly new to RFID tags and thus keep this very simple:
I would be interested in using RFID tags in a closed circulating system for volume control, where I would dropp about 20-100 RFID, which would then have to pass various restrictions of up to 13/32". Temperatures are fairly benign at max. 30ºC and the fluid can either be based on water or diesel. When the tags return I would like to measure them and from the time it took them to complete the circle - assess the system volume. My major concern at the moment is that this would ahppen in an industrial environment, thus plenty of steel around.
Any advice would be appreciated
Daniel