I am having trouble writing to a RF430CL330H type 4 tag from the DLP-RFID2 writer. Here is my original post:
e2e.ti.com/support/wireless_connectivity/nfc_rfid/f/667/t/509685
I've attached 2 logic analyzer captures using the Salae logic analyzer. After a lot of testing, I came to the conclusion that the DLP_RFID2 can write 30 bytes and under successfully in the NDEF payload. If I want to write 31 bytes and above, the DLP-RFID2 won't reply. Is this a firmware bug? Is there any way around this? I've contacted DLP Design directly and they said to post here to get help.
ps - I know the problem is not the RF430CL330H, because it works with the DLP7970ABP with 50+ bytes, and with NDEF messages less than 30 bytes on the RFID2