Hello,
Please assume the Rfdet_h2 = Rfdet_h1= Rfdet = 0. Then, Is the IC enabled or disabled ?
DS p49: 'Not active'
DS p70: 'detection is off.'
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Please assume the Rfdet_h2 = Rfdet_h1= Rfdet = 0. Then, Is the IC enabled or disabled ?
DS p49: 'Not active'
DS p70: 'detection is off.'
Hello Hideaki,
The IC is not controlled by these bits, only by EN and EN2.
The terms "not active" and "detection is off" refer only to the Target Detection feature and nothing else.
On Page 49, the register table also lists "detection is switched off' - the table below it (6-16) just lists out in more detail what the thresholds are.