Hello,
I have the DLP Design NFC/RFID BoosterPack (DLP-7970ABP) booster pack connected to the MSP430F5529 USB LaunchPad.
The launchpad is connected to a laptop by USB and I'm using the software Stollmann NFC Player to detect, red/write on tags.
What I'm trying to do now is to connect the launchpad (with the booster pack) to another dev board using the serial port.
according to the manual:
My understanding is that the serial port is routed to the USB controller and it's possible to isolate it by removing the jumper TXD and RXD
I removed the 2 jumpers but Stollmann NFC Player still work properly and can detect tags.
I would like to keep the USB cable connected to the launchpad to provide the 5V and 3.3V.
I tried to connect a USB serial cable (RX\TX) (COM 25 for Windows)
to P3.3 and P3.4 and tried to and setup NFCPlayer to connect on port 25 but it doesn't connect.
Is there a way to connect the launchpad using the serial port to connect to the laptop or to another target?
Thanks for your help