Other Parts Discussed in Thread: TIMAC, , MSP430F5419A, CC2592
Tool/software: TI-RTOS
Hi,
I'm using TIMAC 1_05_02_43299 and tirtos_simplelink_2_11_01_09.
The CC2650 communicates with another MCU over the UART.
In MSA_ProcessEvent() function I receiver an RF packet and send it over the UART using UART_write(). The other MCU responds but CC2650 is always missing the first byte.
The uart runs in read callback mode but it never gets interrupt to read the first byte.
UART_write is running in blocking mode.
The first byte from the response comes 200 us after data is transmitted. The rest come a few ms later.
Any ideas?
Thanks