Hi Team,
I have downloaded the TI 15.4 stack to utilize the Frequency Hoping concept.
I am using the CC1310 Launchpad.
I can execute the Collector Sensor example provided.
But when I try to run one collector and two sensors both the sensors are getting detected on same channel one after another rather than both sensors getting detected simultaneously on different channel (as per the frequency hoping concept).
Initially I thought it might to do with the settings in the feature.h file and the config.h file.
so modified below stuff:
#define CONFIG_FH_ENABLE false to true in config.h file
and made #define FEATURE_ALL_MODES to #undef FEATURE_ALL_MODES
and made #undef FEATURE_FREQ_HOP_MODE to #define FEATURE_FREQ_HOP_MODE
But doing so now none of the sensors are getting detected by the collector.
Would request to assist on how I can run the frequency hoping example in TI 15.4 stack as I would like to use the Frequency Hoping concept in my firmware for radio transmission.
Thank you
Vikram