Other Parts Discussed in Thread: CC1190
I have tested on our custom hardware and on multiple launchpads and have found there is modulated images at +-24MHz, +-48MHz, +-72MHz, +-96MHz etc that are mixing products from the 24MHz clock transmission internal to the CC1310. The worst of these is -96MHz from the fundamental and causes issues with New Zealand certification (with 20dB amplification in line) in the 915 to 928MHz band due to a restricted band from 800 to 915MHz having a -49dBm limit in 100KHz . This was tested using RFstudio version 2.4.2 with standard setup, constant TX and un-modulated carrier to measure directly into a spectrum analyser (after capacitor moved and cable added). The worst level of image was at 6dBm CC1310 output power measured at -72.48dBm but with inconsistent level, it improves above and below this and is at least 13dB better at 12.5dBm output (hit measurement noise floor).
Could someone at TI shed some light on this issue and any way to reduce the level? I am worried about inconsistencies in this level causing failures at certification. I have more information about test setup/results if needed.