Part Number: CC120XEM-868-930-RD
Hi,
I am trying to use the CC1200 in transparent serial mode with an ASK/OOK RF signal.
I try to get the decoded signal to IOCFG0.
For test puropse I did the following:
Reset the device
Select the generic config symbol rate 4.8kps, OOK, RX BW 128Khz
Changed the frequency to 916.5
SYNC_CFG1:SYNC_MODE = 0
IOCFG0 = 9
PREAMBLE_CFG1:NUM_PREAMBLE =0
MDMCFG1:FIFO_EN = 0
PKT_CFG2:PKT_FORMAT = 3
MDMCFG0:TRANSPARENT_MODE_EN=1
I send an SCAL command to calibrate the device
I send an SRX cmd to go in RX mode and I get the following data on IOCFG0 (see attached picture).
in yellow, I have the signal decoded by a CC1101 device configured in tranparent serial mode (note that the signal symbol rate is 100kps).
In green the signal out of the demo kit. I was expecting to have a flat output put I can see
I go to IDLE
Changed MDMCFG2.IPSAMPLER_P to 2
Changed the RX Filter BW to 400 (416.666)
Changed the symbol rate to 100kps and go back to RX I get the following
Why is there all the "noise" on the output of the demo kit,
Is there any specific configuration I should change to avoid toggling of the serial output.
I made a last change, I removed the antenna and got this.