I have an application that requires connecting 25 peripherals to a Windows host computer wirelessly. The peripherals are all located within 10 meters of the host computer. The peripherals need to send data at a rate of 300 kbps (~37 kBps) back to the windows host. The peripherals will be battery operated and rechargeable, so low power draw is a consideration. The system will be used for half a day, and then re-charged for half a day. I've ruled out Bluetooth and the various 802.15.4 protocols (ZigBee, 6LowPAN, etc) as the max data rate for these is too close (or below) my target data rate. Wi-fi seems like it would work - I can have lots of connections and the data rate supports my requirement. I'm wondering if any of the sub-GHz protocols would work here. I've never used any of these, and not sure how they would compare to a wi-fi based solution. Any thoughts or advice? Do any of the sub-GHz offerings make sense for this application?
Thanks!