Other Parts Discussed in Thread: CC1200, CC1120
Hello
I have seen elsewhere that Ti quote +/- 1.5dB production variation in output power for the CC1200 device. Please can Ti comment on the min/max for the CC1125, whose typical value is quoted as +15dBm?
In order to be as clear as possible, I am not asking about the change in output power as a function of power supply voltage or frequency. I wish to establish what I might see in a large production run of CC1125 devices when I fix the frequency and I fix Vdd ... will there be some variation in Tx power and if so, to what degree ?
Thanks for advice
EB