Hi
Is that possible the power of flashing overlap the power of WiFi packet sending when my application operates file and write something after my device connected to an AP?
If yes, my application should consider to write flash after disconnect AP.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Is that possible the power of flashing overlap the power of WiFi packet sending when my application operates file and write something after my device connected to an AP?
If yes, my application should consider to write flash after disconnect AP.
Hi Jan
My question is
is that any possible flash writing and wifi packet sending happen at same time?
For an extreme example, after sl_WlanConnect function called, my application executes a file write.
If they can happen at same time, the current peak will be higher than current peak of single packet sending.
Should I consider this in my application?
Thanks
Hi Jan
What is the calibration process? RF calibration? When does it execute? AP connecting?
Thanks