Other Parts Discussed in Thread: CC3200
Tool/software: Code Composer Studio
I am having problems with the OTA update example in SDK 1.3.0.
I have setup Dropbox and modified the example code as detailed in the OTA Application Note.
I have read through the answers to similar questions in this forum, and have implemented the changes to ota_api.h & main.c suggested in this response.
When I press SW3 the update appears to download ok and the LP reboots but the App Version shown in the terminal does not change.
Any advice would be most appreciated.
Thanks
Paul.
Project Details
Dropbox configuration
- Vid00_Pid00_Ver0000 : f80_sys_mcuimgA.bin (App version defined as 0.0.1)
UniFlash
- Format
- Apply Service Pack : servicepack_1.0.1.11-2.9.0.0.bin
- /sys/mcuimg.bin : \cc3200-sdk\example\application_bootloader\ccs\Release\application_bootloader.bin
- /sys/mcuimg1.bin : ota_update_nonos\Release\ota_update_nonos.bin (App version defined as 0.0.0)
Terminal Output
************************************************* CC3200 OTA Update Application ************************************************* App Version : 0.0.0 Nwp Version : Wifi Status : Power Off NTP Server : dmz0.la-archdiocese.net NTP Server IP : 0.0.0.0 GTM Time : - Local Time (+05:30) : - OTA Update Status : Press SW3 : Updates or SW2: Factory Reset Run Stat : 0 ************************************************* CC3200 OTA Update Application ************************************************* App Version : 0.0.0 Nwp Version : 2.9.0.0.31.1.4.0.1.1.0.3.37 Wifi Status : Connecting... NTP Server : dmz0.la-archdiocese.net NTP Server IP : 0.0.0.0 GTM Time : - Local Time (+05:30) : - OTA Update Status : Press SW3 : Updates or SW2: Factory Reset Run Stat : 0 ************************************************* CC3200 OTA Update Application ************************************************* App Version : 0.0.0 Nwp Version : 2.9.0.0.31.1.4.0.1.1.0.3.37 Wifi Status : Connected to SC_Home NTP Server : dmz0.la-archdiocese.net NTP Server IP : 0.0.0.0 GTM Time : - Local Time (+05:30) : - OTA Update Status : Press SW3 : Updates or SW2: Factory Reset Run Stat : 0 ************************************************* CC3200 OTA Update Application ************************************************* App Version : 0.0.0 Nwp Version : 2.9.0.0.31.1.4.0.1.1.0.3.37 Wifi Status : Connected to SC_Home NTP Server : dmz0.la-archdiocese.net NTP Server IP : 209.151.225.100 GTM Time : - Local Time (+05:30) : - OTA Update Status : Press SW3 : Updates or SW2: Factory Reset Run Stat : 0 ************************************************* CC3200 OTA Update Application ************************************************* App Version : 0.0.0 Nwp Version : 2.9.0.0.31.1.4.0.1.1.0.3.37 Wifi Status : Connected to SC_Home NTP Server : dmz0.la-archdiocese.net NTP Server IP : 209.151.225.100 GTM Time : Tue Aug 23 2017 11:14:49 Local Time (+05:30) : Tue Aug 23 2017 16:44:49 OTA Update Status : Press SW3 : Updates or SW2: Factory Reset Run Stat : 0 ************************************************* CC3200 OTA Update Application ************************************************* App Version : 0.0.0 Nwp Version : 2.9.0.0.31.1.4.0.1.1.0.3.37 Wifi Status : Connected to SC_Home NTP Server : dmz0.la-archdiocese.net NTP Server IP : 209.151.225.100 GTM Time : Tue Aug 23 2017 11:11:29 Local Time (+05:30) : Tue Aug 23 2017 16:41:29 OTA Update Status : In Progress... Run Stat : 0 ************************************************* CC3200 OTA Update Application ************************************************* App Version : 0.0.0 Nwp Version : 2.9.0.0.31.1.4.0.1.1.0.3.37 Wifi Status : Connected to SC_Home NTP Server : dmz0.la-archdiocese.net NTP Server IP : 209.151.225.100 GTM Time : Tue Aug 23 2017 11:11:29 Local Time (+05:30) : Tue Aug 23 2017 16:41:29 OTA Update Status : Completed Run Stat : 2 : Rebooting... ************************************************* CC3200 OTA Update Application ************************************************* App Version : 0.0.0 Nwp Version : Wifi Status : Power Off NTP Server : dmz0.la-archdiocese.net NTP Server IP : 0.0.0.0 GTM Time : - Local Time (+05:30) : - OTA Update Status : Press SW3 : Updates or SW2: Factory Reset Run Stat : 0