Hi,
I am downloading files with the DropBox V2 API. I want to download some files as well as the service pack. When I point the downloader at the directory with the files I get the following response:
CdnDropbox_SendReqDir: uri=/2/files/list_folder
metadata file=/Vic11/f80_www_logo.png, size=18406
metadata file=/Vic11/f80_www_main2.html, size=5747
metadata file=/Vic11/f43_sys_servicepack.ucf, size=31348
metadata file=/Vic11/f80_sys_mcuimgA.bin, size=144988
metadata file=/Vic11/f00_sys_servicepack.sig, size=256
sl_extLib_OtaRun: OtaClient_UpdateCheck, numUpdates=5
[00:00:14.0344] OTA run (0)
It then proceeds to download the files in the order listed. This causes a problem because the download of the .ucf file will occur (and subsequently fail) before the .sig file. The download of the .ucf file needs to read the .sig file to be sure the signature is correct. If the files are downloaded in the opposite order it works as expected. I have renamed the .sig to f00 and f80 and neither works.
Am I missing something here? I can go through the list and sort them so that the .sig comes first, but I wanted to be sure there was not something I need to do.
Thanks,
Vic