Tool/software: Linux
Hi,
We are certificating our car Head Unit product with wl1831MOD.It's failed in direct case 6.1.10.
Our platform is imx6dl,linux4.1.15.The wifi driver is get from linux 4.1.15 kernel source code.
log of loading wifi driver:
wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[ 3865.260373] wlcore: loaded
[ 3865.727480] wlcore: PHY firmware version: Rev 8.2.0.0.237
[ 3865.774754] wlcore: firmware booted (Rev 8.9.0.0.70)
************************************************************************************************************
I have add some log in wpa_supplicant,and try as follow:
1 set Head Unit(our product with TI WL1831MOD called A) as auto Go
2 smart phone Nexus 6p connect to Head Unit
3 Another Head Unit (called B) with broadcom wifi module witch have certificated connect to smart phone by p2p_connect
4 Connect failed and B will send Device Discoverability Request to A.
5 The log in wpa_supplicant function:wpa_supplicant_event p2p_rx_p2p_action shows that wpa_supplicant didn't receive any Action frame p2p Device Discoverability Reponse.
So I think It's bug of driver or firmware.
Please help me to fix this bug,Thank you very much.