Tool/software: Linux
I am trying to use the calibrator tool, and getting the following error message:
# calibrator --debug wlan0 plt power_mode on
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 68
.type = 2 <ERROR>
.flags = 0 <>
.seq = 13174
.port = 264241396
[ERRORMSG] 20 octets
.error = -95 "Operation not supported"
[ORIGINAL MESSAGE] 16 octets
.nlmsg_len = 16
.type = 21 <0x15>
.flags = 5 <REQUEST,ACK>
.seq = 13174
.port = 264241396
--------------------------- END NETLINK MESSAGE ---------------------------
command failed: Operation not supported (-95)
I've followed the steps described at this link: http://processors.wiki.ti.com/index.php/WL18xx_System_Build_Scripts#Build_Guide