Part Number: BEAGLEBK
Tool/software: Linux
I built a cutomer board based on beagle bone black but added the wl1835 for wireless. I hope the customer board can use both wired and wireless network simultaneously.
Now I can boot the linux with wired network well. But when I add the wireless overlay in uEnv.txt in RED as below.
#Docs: elinux.org/Beagleboard:U-boot_partitioning_layout_2.0
uname_r=4.4.91-ti-r133
#uuid=
#dtb=
###U-Boot Overlays###
###Documentation: elinux.org/Beagleboard:BeagleBoneBlack_Debian
erlays
###Master Enable
enable_uboot_overlays=1
###
###Overide capes with eeprom
#uboot_overlay_addr0=/lib/firmware/<file0>.dtbo
#uboot_overlay_addr1=/lib/firmware/<file1>.dtbo
#uboot_overlay_addr2=/lib/firmware/<file2>.dtbo
#uboot_overlay_addr3=/lib/firmware/<file3>.dtbo
###
###Additional custom capes
uboot_overlay_addr4=/lib/firmware/BB-BBGW-WL1835-00A0.dtbo
#uboot_overlay_addr5=/lib/firmware/<file5>.dtbo
#uboot_overlay_addr6=/lib/firmware/<file6>.dtbo
.....................
The board booted with wrieless network well but there was no eth0 interface anymore.
After I commented the RED line in uEnv.txt the eth0 interface showed again and work well.
Could someone tell me what I should do to make both wired and wireless network work simultaneously ?
Thank you very much.