Other Parts Discussed in Thread: CC2538, Z-STACK, CC3100
Greetings All,
I am working on connecting CC2538EM to another TI module through SPI. I found that there are 2 SSI modules in the CC2538EM. So I searched for the difference between SSI and SPI and found that SSI is somehow more general but I have some questions if someone could help.
Q1) Is there many modifications (functions to be written) that I should do in order to connect an SSI module to SPI module?
Q2) How does the CC2538 connects to SmartRF06, is it through SPI?
Q3) If the answer to Q2 is yes, then which pins are used for this connection from P1 and P2 on the CC2538EM?
Q4) If the answer to Q2 is yes, which SSI module is used for this connection (SSI0 or SSI1)? and is it reserved for only the connection to the SmartRF06 or could I use it further -after flashing my program- to interface to the another slave module of mine?
Q5) If the other module wants 2 more wires (nHIB - HOST_IRQ) more than the standard 4 wires of SPI (MOSI-MISO-CLK-CS) for the connection, should I use 2 GPIOs or there is a better way?
Q6) I read in "Z-stack ZNP Interface Specification" in Z-stack 1.2 that it used 2 additional wires to the default 4 SPI wires, MRDY and SRDY which I think are the same as NHIB and HOST_IRQ, So am I right about this or not?
Thanks in advance
Regards
James