This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDC5801A: Delay control with CDC5801A

Part Number: CDC5801A


I bought a CDC5801A for the purpose of generating the phase-locked RF signal with arbitrarily delay.

Here is my use;

1. I input the RF signal (82.5 MHz) to the "REFCLK".

2. I get the multiplied or divided RF signal from the "CLKOUT/CLKOUTB". 

Then, I want to control the delay of CLKOUT vs REFCLK, but I couldn't understand the function of DLYCTRL.

According to the manual, when CLKOUT = 50 MHz in the "Divide by 2" situation, step delay size is 6.5 ps.

In this case, if I input the 10 rising edges to the DLYCTRL, is the delay with 65 ps generated?

If this is correct, should I prepare some RF source and counter for controlling the delay size?

Sincerely,