This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60400: Low Voltage Automotive Inverter to replace Maxim's MAX16945? (5.4 -> -5.4V is current solution)

Part Number: TPS60400
Other Parts Discussed in Thread: TPS82130, TPS62160-Q1, TPS62150A-Q1, TPS62170-Q1

Hello,

 

I need help replacing a Maxim power part for an automotive customer's radar system.

Their current design uses the MAX16945TGUT/V+ for their -5.4V supply. Here is the datasheet for the Maxim part: Datasheet.  My goal is to pitch one of our parts to replace the Maxim part.  I found one series at TI that is close to what I’m looking for:

  • TPS6040xx

However, it's not a great fit.  The 5.4V input exceeds the recommended Vin range.  Also, the max output is -5V. I’m looking for something that can output at least -5.4V.  I haven’t been able to find any other automotive grade devices that are able to do this low voltage inversion.  Is anyone aware of a device that could replace the current MAXIM part?  

 

 

Best,

Alex