Other Parts Discussed in Thread: INA293, OPA2836, LM7705
Hi,
I have a 4 switch buck boost circuit, as the input/out voltage are in 200V, it is hard to find current sensing amplifier to withstand that voltage, I am thinking to put the sensing resistor at low side, in series with the low side switches, as shown in position A and B. Since both input side and output side are earth grounded, so position C is not possible.
I am wondering if you have reference designs similar to this, and if you can recommend an amplifier for it.
Also the minimum switching frequency is 400kHz, thinking push to 1MHz.
Thanks!