Part Number: THS4551
Other Parts Discussed in Thread: TINA-TI, LMH6550,
Tool/software: TINA-TI or Spice Models
Hi,
I'm have a circuit that I want to replace some op amps with TI pars. I have the whole circuit already simulated in LTspice, but I can't get the imported OP-AMP to work in simulation. I get
ERROR: Node U1:I0:I0:I19:1:102 is floating and connected to current source G:U1:I0:I0:I19:1:RA
ERROR: Node U1:I0:I0:I19:1:302 is floating and connected to current source G:U1:I0:I0:I19:1:RC
ERROR: Node U1:I0:I0:I21:1:102 is floating and connected to current source G:U1:I0:I0:I21:1:RA
ERROR: Node U1:I0:I0:I32:NET8 is floating and connected to current source G:U1:I0:I0:I32:RCMFBAVG1
I tried saving the model as shown in
but no luck.
I have done this before with lmh6550 and it simulates no problem. But the files, when i inspect them in text editor, are different in structure. See both files attacked.
* BEGIN MODEL LMH6550 *////////////////////////////////////////////////////////////////////// * (C) National Semiconductor, Corporation. * Models developed and under copyright by: * National Semiconductor, Corporation. *///////////////////////////////////////////////////////////////////// * Legal Notice: * The model may be copied, and distributed without any modifications; * however, reselling or licensing the material is illegal. * We reserve the right to make changes to the model without prior notice. * Pspice Models are provided "AS IS, WITH NO WARRANTY OF ANY KIND" *//////////////////////////////////////////////////////////////////// *//////////////////////////////////////////////////////////////////// * For more information, and our latest models, * please visit the models section of our website at * http://www.national.com/models/ *//////////////////////////////////////////////////////////////////// *MODEL FEATURES INCLUDE OUTPUT SWING, OUTPUT CURRENT *THRU THE SUPPLIES, GAIN AND PHASE, CLOSED LOOP BANDWIDTH, *SLEW RATE, COMMON MODE REJECTION WITH FREQUENCY EFFECTS, *POWER SUPPLY REJECTION, INPUT VOLTAGE NOISE WITH 1/F, *INPUT CURRENT NOISE, INPUT BIAS CURRENT WITH TEMPCO, *INPUT OFFSET AND TEMPCO, VCM INPUT OFFSET AND TEMPCO, *ENABLE WITH ON AND OFF DELAYS, OUTPUT IMPEDANCE, CLOAD *EFFECTS, VCM SLEW RATE, BALLANCE ERROR VS FREQUENCY, *OUTPUT SHORT CIRCUIT CURRENT, AND QUIESCENT SUPPLY CURRENT. *///MODEL TEMP RANGE IS -40 TO +85 DEG C./// *////////////////////////////////////////////////////////// * PINOUT ORDER -IN VCM V+ +OUT -OUT V- EN +IN * PINOUT ORDER 1 2 3 4 5 6 7 8 .SUBCKT LMH6550 1 2 3 4 5 6 7 8 Q62 183 183 185 QP Q63 186 182 183 QP R70 185 3 2E3 Q64 186 103 187 Q R71 6 187 2E3 Q65 103 103 188 Q Q66 3 186 103 Q R72 6 188 2E3 Q67 189 103 190 Q R73 6 190 1960 Q68 104 104 191 QP Q5 6 117 116 QP R7 118 117 40 Q6 6 119 115 QP 2 Q7 3 112 118 Q 2 Q8 118 102 120 Q 2 R8 6 120 250 Q9 119 102 121 Q 2 R9 6 121 250 Q17 124 104 130 QP 4 Q18 127 103 131 Q 4 R16 6 131 492 C1 115 101 0.83E-12 C2 118 102 0.83E-12 Q19 3 132 133 Q Q20 134 105 135 QP 2 R17 135 3 252 Q21 136 105 137 QP 2 R18 137 3 250 Q22 105 105 138 QP R19 138 3 500 R20 134 132 40 R21 5 133 2 R22 139 5 2 Q23 6 140 139 QP R23 141 140 40 Q24 6 142 134 QP 2 Q25 3 136 141 Q 2 Q26 141 106 143 Q 2 R24 6 143 250 Q27 142 106 144 Q 2 R25 6 144 250 Q28 106 106 145 Q R26 6 145 500 R27 142 136 24 Q35 147 104 155 QP 4 Q36 150 103 156 Q 4 R32 6 156 492 C3 134 105 0.83E-12 C4 141 106 0.83E-12 R33 149 126 200 R34 110 3 585 Q37 105 157 158 Q Q38 159 159 160 QP R36 160 3 800 R37 2 3 60E3 Q39 106 157 109 QP Q40 161 162 109 QP 2 R58 169 7 6E3 R59 7 3 20E3 Q1 3 107 108 Q Q2 109 104 110 QP 2 R1 111 3 252 Q3 112 101 113 QP 2 R2 113 3 250 Q4 101 101 114 QP R3 114 3 500 R4 115 107 40 R5 4 108 2 R6 116 4 2 R69 6 180 5.4E3 Q51 6 169 172 QP Q52 172 173 174 QP R60 174 3 1E3 R61 175 3 1E3 Q53 173 173 175 QP R62 176 173 15.8E3 R63 168 3 33.5E3 Q54 176 177 178 Q R64 6 171 8E3 R65 6 178 250 Q55 170 170 177 Q 2 Q56 179 170 180 Q Q57 177 180 6 Q Q29 6 146 147 QP Q30 105 148 149 Q R28 148 147 40 Q31 3 146 150 Q R38 163 162 200 R39 163 4 2.5003E3 R40 5 163 2.5E3 R41 2 157 200 Q41 102 164 109 QP Q42 101 164 158 Q R42 164 2 200 Q43 159 165 158 Q 2 Q44 161 161 166 Q R43 6 166 800 Q45 158 103 167 Q 2 R44 6 167 500 R45 6 2 60E3 R46 165 163 200 Q46 115 101 111 QP 2 Q49 6 168 169 QP Q50 168 170 171 Q Q32 106 151 149 QP R29 151 150 40 Q33 6 152 153 QP 1.01 R30 154 3 492 R31 155 3 492 Q34 153 104 154 QP 4 Q58 180 177 181 Q 2 R66 170 3 84E3 Q59 3 176 179 Q Q60 182 172 179 Q Q61 182 183 184 QP R67 184 3 2E3 R68 6 181 1150 R74 191 3 2E3 Q69 189 104 192 QP R75 192 3 2E3 Q70 6 189 104 QP C5 170 6 0.5E-12 I1 146 152 1.2E-6 I2 123 8 1.2E-6 E2 146 0 153 0 0.99986 V33 152 1 -100E-6 Q10 102 102 122 Q R10 6 122 500 R11 119 112 24 Q11 6 123 124 QP Q12 101 125 126 Q R12 125 124 40 Q13 3 123 127 Q Q14 102 128 126 QP R13 128 127 40 Q15 6 8 123 QP R14 129 3 492 R15 130 3 492 Q16 123 104 129 QP 4 .MODEL Q NPN BF=179.3 VAF=68 RB=80 KF=1E-16 IKF=0.1 .MODEL QP PNP BF=105.95 VAF=68 RB=80 KF=1E-16 IKF=0.1 .ENDS * END MODEL LMH6550
Is there a way I can import/convert the THS4551 model? Or am I just importing it wrong?
Best regards,
Marko