This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/THS4551: Importing model to LTspice

Part Number: THS4551
Other Parts Discussed in Thread: TINA-TI, LMH6550,

Tool/software: TINA-TI or Spice Models

Hi, 

I'm have a circuit that I want to replace some op amps with TI pars. I have the whole circuit already simulated in LTspice, but I can't get the imported OP-AMP to work in simulation. I get 

ERROR: Node U1:I0:I0:I19:1:102 is floating and connected to current source G:U1:I0:I0:I19:1:RA
ERROR: Node U1:I0:I0:I19:1:302 is floating and connected to current source G:U1:I0:I0:I19:1:RC
ERROR: Node U1:I0:I0:I21:1:102 is floating and connected to current source G:U1:I0:I0:I21:1:RA
ERROR: Node U1:I0:I0:I32:NET8 is floating and connected to current source G:U1:I0:I0:I32:RCMFBAVG1

I tried saving the model as shown in 

but no luck. 

I have done this before with lmh6550 and it simulates no problem. But the files, when i inspect them in text editor, are different in structure. See both files attacked. 

* BEGIN MODEL LMH6550
*//////////////////////////////////////////////////////////////////////
* (C) National Semiconductor, Corporation.
* Models developed and under copyright by:
* National Semiconductor, Corporation.  
*/////////////////////////////////////////////////////////////////////
* Legal Notice:  
* The model may be copied, and distributed without any modifications;
* however, reselling or licensing the material is illegal.
* We reserve the right to make changes to the model without prior notice. 
* Pspice Models are provided "AS IS, WITH NO WARRANTY OF ANY KIND" 
*////////////////////////////////////////////////////////////////////
*////////////////////////////////////////////////////////////////////
* For more information, and our latest models,
* please visit the models section of our website at
*       http://www.national.com/models/
*////////////////////////////////////////////////////////////////////
*MODEL FEATURES INCLUDE OUTPUT SWING, OUTPUT CURRENT
*THRU THE SUPPLIES, GAIN AND PHASE, CLOSED LOOP BANDWIDTH,
*SLEW RATE, COMMON MODE REJECTION WITH FREQUENCY EFFECTS,
*POWER SUPPLY REJECTION, INPUT VOLTAGE NOISE WITH 1/F,
*INPUT CURRENT NOISE, INPUT BIAS CURRENT WITH TEMPCO,
*INPUT OFFSET AND TEMPCO, VCM INPUT OFFSET AND TEMPCO,
*ENABLE WITH ON AND OFF DELAYS, OUTPUT IMPEDANCE, CLOAD
*EFFECTS, VCM SLEW RATE, BALLANCE ERROR VS FREQUENCY,
*OUTPUT SHORT CIRCUIT CURRENT, AND QUIESCENT SUPPLY CURRENT.
*///MODEL TEMP RANGE IS -40 TO +85 DEG C.///
*//////////////////////////////////////////////////////////
* PINOUT ORDER -IN VCM V+ +OUT -OUT V- EN +IN
* PINOUT ORDER  1   2   3   4    5   6  7   8
.SUBCKT LMH6550 1 2 3 4 5 6 7 8
Q62 183 183 185 QP
Q63 186 182 183 QP
R70 185 3 2E3
Q64 186 103 187 Q
R71 6 187 2E3
Q65 103 103 188 Q
Q66 3 186 103 Q
R72 6 188 2E3
Q67 189 103 190 Q
R73 6 190 1960
Q68 104 104 191 QP
Q5 6 117 116 QP
R7 118 117 40
Q6 6 119 115 QP 2
Q7 3 112 118 Q 2
Q8 118 102 120 Q 2
R8 6 120 250
Q9 119 102 121 Q 2
R9 6 121 250
Q17 124 104 130 QP 4
Q18 127 103 131 Q 4
R16 6 131 492
C1 115 101 0.83E-12
C2 118 102 0.83E-12
Q19 3 132 133 Q
Q20 134 105 135 QP 2
R17 135 3 252
Q21 136 105 137 QP 2
R18 137 3 250
Q22 105 105 138 QP
R19 138 3 500
R20 134 132 40
R21 5 133 2
R22 139 5 2
Q23 6 140 139 QP
R23 141 140 40
Q24 6 142 134 QP 2
Q25 3 136 141 Q 2
Q26 141 106 143 Q 2
R24 6 143 250
Q27 142 106 144 Q 2
R25 6 144 250
Q28 106 106 145 Q
R26 6 145 500
R27 142 136 24
Q35 147 104 155 QP 4
Q36 150 103 156 Q 4
R32 6 156 492
C3 134 105 0.83E-12
C4 141 106 0.83E-12
R33 149 126 200
R34 110 3 585
Q37 105 157 158 Q
Q38 159 159 160 QP
R36 160 3 800
R37 2 3 60E3
Q39 106 157 109 QP
Q40 161 162 109 QP 2
R58 169 7 6E3
R59 7 3 20E3
Q1 3 107 108 Q
Q2 109 104 110 QP 2
R1 111 3 252
Q3 112 101 113 QP 2
R2 113 3 250
Q4 101 101 114 QP
R3 114 3 500
R4 115 107 40
R5 4 108 2
R6 116 4 2
R69 6 180 5.4E3
Q51 6 169 172 QP
Q52 172 173 174 QP
R60 174 3 1E3
R61 175 3 1E3
Q53 173 173 175 QP
R62 176 173 15.8E3
R63 168 3 33.5E3
Q54 176 177 178 Q
R64 6 171 8E3
R65 6 178 250
Q55 170 170 177 Q 2
Q56 179 170 180 Q
Q57 177 180 6 Q
Q29 6 146 147 QP
Q30 105 148 149 Q
R28 148 147 40
Q31 3 146 150 Q
R38 163 162 200
R39 163 4 2.5003E3
R40 5 163 2.5E3
R41 2 157 200
Q41 102 164 109 QP
Q42 101 164 158 Q
R42 164 2 200
Q43 159 165 158 Q 2
Q44 161 161 166 Q
R43 6 166 800
Q45 158 103 167 Q 2
R44 6 167 500
R45 6 2 60E3
R46 165 163 200
Q46 115 101 111 QP 2
Q49 6 168 169 QP
Q50 168 170 171 Q
Q32 106 151 149 QP
R29 151 150 40
Q33 6 152 153 QP 1.01
R30 154 3 492
R31 155 3 492
Q34 153 104 154 QP 4
Q58 180 177 181 Q 2
R66 170 3 84E3
Q59 3 176 179 Q
Q60 182 172 179 Q
Q61 182 183 184 QP
R67 184 3 2E3
R68 6 181 1150
R74 191 3 2E3
Q69 189 104 192 QP
R75 192 3 2E3
Q70 6 189 104 QP
C5 170 6 0.5E-12
I1 146 152 1.2E-6
I2 123 8 1.2E-6
E2 146 0 153 0 0.99986
V33 152 1 -100E-6
Q10 102 102 122 Q
R10 6 122 500
R11 119 112 24
Q11 6 123 124 QP
Q12 101 125 126 Q
R12 125 124 40
Q13 3 123 127 Q
Q14 102 128 126 QP
R13 128 127 40
Q15 6 8 123 QP
R14 129 3 492
R15 130 3 492
Q16 123 104 129 QP 4
.MODEL Q NPN BF=179.3 VAF=68 RB=80 KF=1E-16 IKF=0.1
.MODEL QP PNP BF=105.95 VAF=68 RB=80 KF=1E-16 IKF=0.1
.ENDS
* END MODEL LMH6550
 (originally a .mod file, changed to txt for upload)

THS4551.lib

Is there a way I can import/convert the THS4551 model? Or am I just importing it wrong?

Best regards, 

Marko 

  • Hi Marko,

    Essentially you just select the part in TINA-TI, open its macro file, and save it as a generic “.CIR” file.

    Best regards,

    Sean
  • What you suggested is shown in the video I linked in. If i do that I get the same file as the .lib just the extension is different and I get the same error.
  • Hi Marko,

    I get this error as well, and I will notify the model group. In the meantime, you can always use TINA-TI.

    Best regards,

    Sean
  • Did this resolve your issue? Were you able to use TINA-TI to simulate your circuit? I notice you are in Slovenia, my maternal family is from Polhov gradec. Me veseli!
  • Živjo!

    I tried to use tina but it was to much of a hassle.

    So I tried to fix the model. Some large value resistor between some nodes in the model were added and that got rid of the floating node errors. Than there were some voltage sources with not defined values that were a problem so (assumed) they were set to 0V. 

    Then the model ran in LTspice, but it was really picky. It would give strange results every now and then.E.G. The simulation would not start if I added 1 resistor or change a value of the capacitor. or  E.G. the output of the op amp would go to +5 MV (yes Mega) and above with +3.3 V power supply. I looked at the model some more and there were also some sub circuits that were defined (but form what i could tell) were never used in the model which is strange.

    So I gave up on this chip, as I wasted enough time, and used another chip form AnalogDevices. 

    Best regards, 

    Marko