Other Parts Discussed in Thread: OPA2625, THS4131
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OPA2625, THS4131
And actually Jon, you would use a part like the THS4131 to level shift your input to 0V centered and then only use one side of the output as a single ended in to single out DC adjustment.
Would have to set up for a gain of 2 to get a net gain of 1 if only using one side of output.
here you go Jon, see if this makes any sense,
essentially using the FDA common mode loop to do a DC coupled level shift. It produces a differential output, but you can just use one side - works well it seems. Don't know your load, but match them on each output side.
DC coupled level shift of 250kHz square wave from 18V centered to 0V centered.docx