This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

remove dc offset from signal going into an op amp

Other Parts Discussed in Thread: OPA2625, THS4131

I have a signal that varies between 19V and 17V @ 250kHz. The signal operates in a burst pattern where it outputs 2048 values then stops for a few ms. I want to input this signal into an op amp and remove the dc level. I have a circuit that has a dc blocking capacitor between the signal and the op amp input. The op amp is set as a buffer, and also has a resistor to ground. So I have a high pass filter on the input of the buffer. The issue I have is that I am finding that the circuit takes a long time to settle if I select values that maintain the signal integrity. If I then change the values to speed up the settling time the signal starts to degrade. Are there any other options that will maintain the signal integrity whilst giving a fast settling time? I am open to using a completely different circuit. Thanks