Other Parts Discussed in Thread: LM1876 , LM4935 , OPA1662 , OPA1664 Blast from the Past! 1980 NSC Audio/Radio Handbook!
Howdy,
We've gotten several requests for this, so here it is!
Sorry the scan isn't 100% clear, but the print quality of the…
Other Parts Discussed in Thread: TAS5768M , TAS5766M , TAS5756M , TAS5782M Tool/software: Linux
Linux Driver for TAS5766M and TAS5768M
Below is a Linux ALSA driver for TAS5766M and TAS5768M. This driver is kept as simple as possible. Its major purpose…
How to revive a MC57xxPSIA board
The MC57xxPSIA is a board used to interface, configure and control the TAS57xx family of digital audio amplifiers.
The Firmware of the MC57xxPSIA may get corrupted, resulting in Windows not recognizing the board…
Other Parts Discussed in Thread: DRV601 , DRV603 , DRV602 , DRV632 , TINA-TI DRV601 vs DRV603 design/layout differences
Q: DRV601 vs DRV603 design/layout differences
Customer is looking at the design / layout differences between the DRV601 and DRV603…
Other Parts Discussed in Thread: TPA711 , TAS5630 , TAS5615 , TAS5613 Class AB amplifier efficiency in SE configuration
Q: Class AB amplifier efficiency in SE configuration
A customer wants to use a TPA711 in SE mode to drive a 15 Ohm speaker. Could…
Part Number: TMS320C5517
The C55x CSL has an example that demonstrates waking-up the DSP core from IDLE3 via RTC.
This is an example that demonstrates waking up from IDLE3 via the INT0 pin on the C5517 using the EVM5517.
Instructions for running…
Part Number: MSP-GANG
Hello!
We are excited to announce a new software update for the MSP-GANG device! Thanks to this new update, programming times have dropped by a substantial amount (up to 32.1% on certain devices)!
For those of you who may not…
Other Parts Discussed in Thread: SN74LVC1G08 FAQ: Logic and Voltage Translation > Output Parameters >> Current FAQ
Very few logic devices specify an output transition rate, and those that do only specify it under very specific conditions.
The best…