Part Number: AM6442 Other Parts Discussed in Thread: TMDS64EVM
Tool/software:
AM64x boot ROM supports booting from parallel GPMC NAND. From "4.4.10 GPMC NAND Boot" in AM64x TRM "AM64x ROM only supports boot from ONFI 1.0 compatible 8 bit parallel…
Part Number: TMUX1574
Tool/software:
Shoot-through current occurs when CMOS inputs are somewhere between their High and Low voltages, effectively turning on both MOSFETs in the CMOS structure. In many devices, including analog multiplexers, this creates…
Other Parts Discussed in Thread: SYSCONFIG The DDR Controller and PHY in Sitara processors is a flexible interface which can be used with LPDDR4 or DDR4. There are many settings available to fine-tune the signal timing on this interface. These settings…
Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: SK-AM62-LP , SK-AM62A-LP
Tool/software:
Hi
I want to use the DDR Margin Test Tool on the AM62x-SK-EVM for testing, but I encountered an issue in the red step while following the readme…
Part Number: PROCESSOR-SDK-AM64X
Tool/software:
Hi Team,
I want to use two AM64x board for PCie communication.
One EVM acts as root complex and other EVM acts as a Endpoint. I am using PE-FLEXI-G2-MMCX-12-TII.
I want to verify memory read…