Part Number: TDA4VM In the rti_app_uc(1-4) and the rti_test_app tested on SDK 8.6, 9.0 and 9.1, the interrupt callback is received much before the wait delay in the code sequence. The program does not wait for the callback to be triggered.
Observed…
Part Number: TDA4VM Hello,
We need a CAN example which runs on MCU2_1 with freeRTOS OS along with Linux running on A72 with SPL boot flow and also the CAN instance used in CAN example has to be MCAN0( Main domain CAN0).
SDK version: 9.1
Regards…
Part Number: AM62A7
Could you confirm that the voltage domains are correct for the MMC1_SDCD and MMC1_SDWP pins? The datasheet shows both MMC0 and MMC2 as having all member pins bellowing to the same voltage domain. For MMC1 however, the pins are shown…
Other Parts Discussed in Thread: SYSCONFIG , TDA4VH TI’s SysConfig PinMux Tool is a GUI interface which allows the user to select the desired device pin configurations for their system. The SysConfig PinMux Tool outputs customer-selected configurations…
Other Parts Discussed in Thread: C2000WARE Below Errata Advisory is applicable for TMS320F28003x,TMS320F28004x devices with more than one flash bank. We will add this advisory to the respective device errata document soon. Also, we will update the flash…
Part Number: C2000WARE What are some common issues that arise when porting over old C2000WARE versions to the newest C2000WARE versions? How can I resolve them?
Part Number: MSPM0-SDK Other Parts Discussed in Thread: SYSCONFIG , MSPM0G3507
Environment:
1. CCS: 12.6.0.00008
2. SysConfig: 1.19.0
3. MSPM0 SDK: 1.30.00.03
Stpe 1: Import a project from SDK and Rebuild project: empty_LP_MSPM0G3507_nortos_ticlang…
Part Number: AM623
Team,
A few more questions about decoupling as I couldn’t find anything in the TI documentation regarding some pins of the AM62X:
Do the following pins need their own decoupling capacitors (it doesn’t look like the TI EVM had…