Part Number: MSPM0G3519
This E2E thread contains reference application codes for the Application Note titled- Advanced Timer Techniques in MSPM0.
Advanced Timer (TIMA) peripherals in MSPM0 Devices are designed to meet the demands of modern embedded…
Part Number: AM2634 Other Parts Discussed in Thread: SYSCONFIG
In this FAQ, I explain an approach to transmit a large amount of data from an AM263x SPI slave device while keeping the chip select (CS) deassertion time to a minimum.
Part Number: AM625
The new Boots Quirk Function, Flash_quirkSpansionSafebootDetection , introduced in MCU+ SDK 11.02, is specifically designed for Serial NOR Flash devices (S28HS512T and S25HL512T). If you are using custom Flash parts, you must modify…
Part Number: TDA4VH-Q1
When a user presses Ctrl-C to stop the application, the default behavior sets a shutdown flag but may not perform proper cleanup. The main application thread could be blocked waiting for messages from the remote cores (R5F, C7x…
FAQ: Logic and Voltage Translation > > Current FAQ
[FAQ] What is the Difference Between I2C and SPI I/O Expansion
[FAQ] VOH/IOH/VOL/IOL and Total ICC Current Definitions
Other Parts Discussed in Thread: TMDX654IDKEVM I want to test PRU Ethernet on the AM65x IDK EVM (TMDX654IDKEVM).
I am using Linux SDK 11.2. I am booting the default filesystem image, tisdk-default-image-rt-am65xx-evm-11.02.05.02.rootfs.wic.xz. However…
Part Number: TMS320F28P550SJ
Hello,
I followed outlined steps in gain calibration section of TRM chapter, but for some reason my ADCRESULT register does not show 0.9 * VREFHI, but a floating value. What could be the reason?
Part Number: TMS320F28P550SJ
I had an issue with ADC Zero Offset calibration. I followed steps outlined in TRM, but for some reason my Vreflo ADCRESULTREG keeps showing zero instead of certain offset. Could you help me with this issue, please?
Part Number: CC2745R10-Q1 Other Parts Discussed in Thread: CC2755R10
This post presents three example projects demonstrating incremental BLE functionality on the TI CC2755 microcontroller using Zephyr 3.7.0 v3.7.0-ti-9.14.00_ea.
All projects use:…