Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Greetings,
Currently on the AM62x TI EVM, there is an OSPI flash part integrated.
The OSPI Flash is S28HS512T.
If we want to interface QSPI Flash part…
Part Number: AM62D-Q1 Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi TI Experts,
Do you have recommendations on using MCASP Audio peripheral?
Part Number: AWRL1432BOOST-BSD Tool/software: Due to the BSD's demo large number of chirps and adc samples there have been issues with raw data capture with the DCA1000. To help alleviate this issue there are two steps to be taken
1) One cannot start…
Part Number: LMH1297
Tool/software:
Hi,
When performing diagnostic evaluations of the LMH1297 retimer customers often want to adjust input cable EQ from the IO side. In these cases we recommend disabling the EQ adaptation and performing the following…
[Click here to return to Transceiver Homepage]
Welcome to the CAN Transceivers E2E page!
Listed below are a variety of resources to assist with the implementation of the Controller Area Network, aka CAN!
Frequently Asked Questions (FAQs):…
Welcome to the Interface Transceivers E2E page!
Here you will find a variety of resources that support our long list of devices (750+ and counting!)
Select an interface below to find a collection of FAQs, application notes, videos, and more: …
Part Number: DS320PR810 Other Parts Discussed in Thread: DS320PR1601 , DS160PR1601
Tool/software:
How do I check to make sure my PCIe signals are AC-coupled correctly?
FAQ: TPLD > Current FAQ
The two biggest causes of slow simulation are:
Fast oscillators and switching signals
Large simulation timescales (simulations that take 1+ seconds)
If the simulation is utilizing a square wave with a period that is…