Tool/software:
Note: Update for CCSv20.2.0. This page will continue to be updated as necessary for relevant information to the FAQ.
Question: Where are the Flash Settings for my device in CCS?
Answer: In order to reach the Flash Settings, proceed…
Part Number: TDA4VL-Q1 Tool/software: Does the SDL ECC test cover error injection tests on the inaccessible endpoints? If not, what is the testing procedure for these endpoints?
Part Number: TDA4VH-Q1 Tool/software: Does the SDL ECC test cover error injection tests on the inaccessible endpoints? If not, what is the testing procedure for these endpoints?
Part Number: AM623 Other Parts Discussed in Thread: AM625
Tool/software:
Usually add RC filter on RESET signal to anti noise, but the slew rate requirement of RESET signal on AM62x datasheet is quite sharp, on customer board it is about 10V-100V/ms…
Part Number: AM623
Tool/software:
#1. Did not find MMC0 HS200 slew rate data in datasheet timing section, so section 7.8.6 LVCMOS Electrical Characteristics data applies?
#2. The Min vale: 18f or 1.8E+6, the two value are quite different, 18f=18x200MHz…
Part Number: DP83848Q-Q1 Tool/software: If the CLKOUT output is not used on DP83848, it may be disabled using the below register writes. This may be beneficial for EMC emissions testing, in order to minimize the energy of 25Mhz harmonics.
0x13[0] =…
When posting a new software inquiry on the TI E2E forum, please follow this guideline for the initial post.
Describing the Problem
Using the following list of questions as the template, copy and paste the questions to your post, and answer them if…
Part Number: AM67A Other Parts Discussed in Thread: SK-AM69 , SK-AM68 , AM67 , SK-TDA4VM Tool/software: How can I enable CSI2 sensors via fusion boards such as Arducam V3Link or fusion 1 daughter board (EVM577PFUSION-V1-0)?
Part Number: AM625
Tool/software:
Dear all,
In AM625: Help setting PRUSS clock to 333MHz on AM6254 I was able to set my AM625's PRU to run at 333MHz and confirmed it with a scope.
Now I'd like to understand whether spread spectrum can be enabled…
Part Number: LP-AM243 Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I am trying to modify the gpio_input_interrupt example for the R5F0-0 core to direct the GPIO interrupt to the PRU core.
Requirement: GPIO1_0 interrupt -> MAIN_GPIOMUX_INTROUTER0_OUTP_18…