Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: TDA4VM
Tool/software:
Hi Expert,
My customer Motovis report an issue about ethernet link down issue, customer have catch the MDIO using the Logic analysis, they find there is some difference…
Part Number: AM625
Tool/software:
Hi Ti Experts,
I am designing a custom board for the AM6254 SoC and trying to connect an SPI peripheral to the AM6254 SPI interface.
I intend to use MCU_SPI1 Channel but I am not sure which one is MISO and MOSI…
Part Number: TUSB2E221 Other Parts Discussed in Thread: TUSB2E22 Tool/software: The TUSB2E221 is the latest 2-port eUSB2 repeater. Released in 2024, it contains updates that allow it to conform to the latest eUSB2 v1.2 specification as well as adding…
Part Number: TDA4AP-Q1
Tool/software:
Hi TI Experts,
Customer is working on TDA4AP SDK10.0. They are using SPL boot.
They want to change the De-emphasis to be -3.5dB for PCIe0 for 5.0GT/s to minimize reflection. Please see the below description…
Part Number: AM2434 Other Parts Discussed in Thread: SYSCONFIG ,
Tool/software:
Hello TI,
is it possible to configure 1.8V and 3.3V domains in SysConfig and select I/O pins according to the preferred voltage?
I have seen a drop-down box for some…
I am using a processor with a DM R5F (AM62x, AM62Ax, AM62Px). I am using SDK 9.2.1 or SDK 10.0. The Device Manager (RM) R5F core is listed in the Linux devicetree, so Linux should use the remoteproc driver to attach to the DM R5F during Linux boot time…
Part Number: SK-AM69 Other Parts Discussed in Thread: SK-AM68 , AM67 , SK-TDA4VM
Tool/software:
Hi,
I have a Starter Kit (SK) Edge AI device with a CSI sensor connected and would like to stream to my display. I have enabled the sensor by following…