Part Number: TPS546B25
To use the FUSION GUI in offline mode with TPS546B25,
use the attached TPS546B25 xml to get started.
Start Fusion GUI,
After scan,
Click Offline Mode
and Load the xml
TPS546B25116.0 Address 17 Project File.xml
Part Number: MSPM0G3519
This E2E thread contains reference application codes for the Application Note titled- Advanced Timer Techniques in MSPM0.
Advanced Timer (TIMA) peripherals in MSPM0 Devices are designed to meet the demands of modern embedded…
Part Number: AM2634 Other Parts Discussed in Thread: SYSCONFIG
In this FAQ, I explain an approach to transmit a large amount of data from an AM263x SPI slave device while keeping the chip select (CS) deassertion time to a minimum.
Part Number: AM625
The new Boots Quirk Function, Flash_quirkSpansionSafebootDetection , introduced in MCU+ SDK 11.02, is specifically designed for Serial NOR Flash devices (S28HS512T and S25HL512T). If you are using custom Flash parts, you must modify…
Part Number: TDA4VH-Q1
When a user presses Ctrl-C to stop the application, the default behavior sets a shutdown flag but may not perform proper cleanup. The main application thread could be blocked waiting for messages from the remote cores (R5F, C7x…
FAQ: Logic and Voltage Translation > > Current FAQ
[FAQ] What is the Difference Between I2C and SPI I/O Expansion
[FAQ] VOH/IOH/VOL/IOL and Total ICC Current Definitions
Other Parts Discussed in Thread: TMDX654IDKEVM I want to test PRU Ethernet on the AM65x IDK EVM (TMDX654IDKEVM).
I am using Linux SDK 11.2. I am booting the default filesystem image, tisdk-default-image-rt-am65xx-evm-11.02.05.02.rootfs.wic.xz. However…
Part Number: TMS320F28P550SJ
Hello,
I followed outlined steps in gain calibration section of TRM chapter, but for some reason my ADCRESULT register does not show 0.9 * VREFHI, but a floating value. What could be the reason?
Part Number: TMS320F28P550SJ
I had an issue with ADC Zero Offset calibration. I followed steps outlined in TRM, but for some reason my Vreflo ADCRESULTREG keeps showing zero instead of certain offset. Could you help me with this issue, please?