Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG
In MCU+ SDK 11.02, the OSPI and Flash examples are configured by default to operate at the highest protocol: 8D-8D-8D. For configuring 8S-8S-8S SDR Protocol on S28HS512T Serial NOR OSPI…
Part Number: TDA4VH-Q1
Hi,
After reset of C7x, i am trying to load newer C7x binary, but the second load takes a lot of time.
Could you please help me to solve this issue.
Part Number: AM6442 Other Parts Discussed in Thread: UNIFLASH
I am trying to flash an image for AM64/AM243 device by loading SBL JTAG UNIFLASH from CCS version 20. *.* , after following the steps mentioned in the MCU+SDK documentation: https://software…
Part Number: BQ25630EVM Other Parts Discussed in Thread: BQ25630 , BQSTUDIO ,
Please see attached for the BQ25630 BQZ file to be used with BQSTUDIO software.
To use the GUI you will need to download Battery management studio software from TI.com,…
Other Parts Discussed in Thread: LP-MSPM0G3507 printf_to_uart_LP_MSPM0G3507_nortos_ticlang.zip
Default UART pin is PA10 and PA11, and it's based on LP-MSPM0G3507 default.
Please check corresponding Launchpad's User guide schematic before test. There…
Part Number: BQ25188EVM Other Parts Discussed in Thread: BQSTUDIO , EV2400 , BQ25188 , BQ25186 , BQ21088
The BQ2518x EVM can be used with the EV2400 and bqStudio. Connect the SDA, SCL, and GND pins on the EVM to the corresponding pins on the EV2400…
Other Parts Discussed in Thread: BQ25186 , BQ21088 , BQ25180 , BQ25188 , BQ25185 , BQ21080 BQ2518x FAQ Home Page
This home page is for common questions in relation to the BQ25188, BQ21088, BQ25185, BQ25186, BQ25180, and BQ21088.
FAQs
----…
Part Number: AM62A7-Q1
Hi,
I am trying to do CPU reset for C7x core on AM62Ax device and facing a page fault error.
Below is the error message.
"(Error -1351 - (0:0:0)) Register or Memory request has timed out. The CPU is executing a High Priority…
Part Number: AM62D-Q1
When implementing audio input/output systems using MCASP (Multichannel Audio Serial Port), there is inherent latency in the audio pipeline(SW) due to buffer priming and the DMA queuing mechanism. This FAQ explains the fundamental…