Part Number: F29H850TU
Why am I getting a Frame Error ( FE = 1 ) on my next LIN transmission immediately after a No-Response Error ( NRE ) occurs?
Can I clear this stuck state by performing dummy reads of the receive buffers ( LINRD0 and LINRD1…
Part Number: MSPM0G3519
This thread is created to presenta an efficient implementation of the ED25519PH elliptic curve cryptography algorithm (from the Libsodium library) optimized for MSPM0G microcontrollers with MATHACL module.
While the ARM Cortex…
Part Number: F29H850DM Other Parts Discussed in Thread: F29H850TU , SYSCONFIG
Key Provisioning is failing on F29H859TU8, F29H859TM8, F29H859DU6, F29H859DM5. Code Provisioning is failing on F29H859TU8, F29H859TM8, F29H859DU6, F29H859DM5.
Part Number: AM625
SYSFW/TIFS supports configuring the firewall on AM6xx SoC https://software-dl.ti.com/tisci/esd/latest/6_topic_user_guides/firewall_faq.html
There're two ways to configure the firewall via TIFS A/. calling the TIFS firewall APIs…
Part Number: DRV8161
VDSLVL will start at one of the seven levels of VDSLVL LEVELx-0 depending on RVDSLVL:
To select a level on the LEVELx-0 levels, all that is required is to select RVDSLVL depending on the level desired; the MCU, diode, and…
Part Number: J721S2XSOMXEVM
In Security Enforced (HS-SE) devices, the JTAG port is closed by default. The below table shows the default state of the JTAG on various device types.
This prevents debugging entirely—even for non-secure cores—until the…